Send clear signals: Directly display operating states with new LED strip

item Innovations 

Brings light into the darkness: The new LED Strip RGB 24V from item enables high-quality signaling solutions and can be easily integrated into profile frames with slot 8. The basic colors can be controlled individually or together. This means that the operating status of systems is always directly visible.

The LED Strip RGB 24V is bright and energy-efficient. It can be controlled via a four-pole connection cable and can light up in different colors. Thus, operating states in production and logistics can be easily displayed. The LED strip is flexible, 3 mm high and available in lengths of 1,000 mm and 2,000 mm. It can be shortened in sections of 100 mm as required. The installation is uncomplicated and quickly realized: The LED strip is simply inserted into an LED sheathing profile 8 14x5. The translucent hollow chamber profile can then be fixed in the groove and thus serves as a secure sheathing for the RGB strip, which also protects it from dirt and damage. The cover cap, which is available especially for the LED sheathing profile, securely closes the end faces and also serves as a strain relief for the cable of the LED strip. This can be easily extended with the sensor/actuator connection cable. The 5 m long four-pole cable has a pre-mounted M12 connection socket. Due to the 24-volt technology, the LED strip can be optimally connected to the controller. This is made possible by the optional M12 A-coded connection plugs, which are even attached to the open cable ends without tools.

As a result, the new LED strip in combination with the coordinated components can be used to implement luminous and highly visible signaling solutions based on classic aluminum profiles.

Further information is available via the ePaper: https://media.item24.com/ePaper/de/item-Neuheiten-2023-I/

Length: 1798 characters including spaces

Date: 14 June 2023

Photos: 2 (source: item)

Caption 1: The new RGB 24V LED strip from item enables high-quality signaling solutions and can be easily integrated into profile frames with slot 8.

Caption 2: The long-lasting, high-luminosity RGB strip can be used to indicate operating states in production and logistics and is optimally protected by the translucent hollow chamber profile.

Dürfen wir Sie persönlich beraten?

Projektanfrage

Wir helfen Ihnen bei der Planung Ihrer Projekte.
Individuell und höchst effizient.

Konfigurieren

Individuell, einfach und jederzeit online planen.

Online Katalog

Jederzeit bequem und einfach bestellen!

de
Sprache
Land
Schweiz
Vertriebspartner finden